How 3D-Machine Vision is Transforming Robotics
Image Source:
Zapp2Photo/Shutterstock.com
By Adam Kimmel for Mouser Electronics
Published May 6, 2021
A high-speed machine experiences a wide tolerance for cutting a hole because of tool wear over the life of a
piece of capital. This tolerance compromises the downstream manufacturing steps leading to a scrap rate of 15
percent. This rate reduces the number of parts the machine produces in a day, so engineers shut it down to
reprogram. The next iteration is better, but the scrap rate is still 8.5 percent. To make up for the downtime
and scrap, the team decides to accept the scrap rate to increase fabrication speed to avoid further downtime to
reprogram. The increased speed improves throughput, but the high tolerance increases the scrap rate to 12
percent. Capacity continues to lag. Soon production is so far behind management must approve another shift and
overtime.
Downtime, reprogram, run, check, repeat.
This cycle now seems to be in a death spiral, hopelessly incapable of catching up to meet the production
schedule. High-speed robotics hinges on accuracy, and the cost of an errant dimensional reading can be
catastrophic. 3D-machine vision has disrupted intelligent robotics by improving the quality, throughput, and
cost of mass manufacturing. Able to react in real-time, this technology auto-corrects and provides feedback to
the operators simultaneously, keeping production running while proactively alerting the robot’s human
counterparts of the issue.
3D-machine vision receives, processes, and reacts to unexpected events during operation and completes its task
without reprogramming to create a fully automated experience. In the following, we explore three manufacturing
tasks handled by robotics—pick and place, outgoing dimensional inspection, and defect
identification—along with how 3D vision solves a known process error that occurs with each.
Pick and Place
As automated outgoing dimensional inspection benefits from the accuracy of 3D-machine vision, the robotics
technology’s flexibility benefits pick and place, a critical process step, especially during a climate
when supply chains everywhere are strained. Software engineers develop algorithms to detect, reach, grab, move,
and place an item for order fulfillment. The enterprise resource planning (ERP) system receives an order from
the system and transmits it to the robotics for product pull.
With an influx of orders, wasted time is lost revenue. If the machine has an improper grabbing force, the robot
can damage the product, losing time and a saleable good in the process. 3D imaging takes a holistic picture of
the product and can feed strength information back to the processor in real-time, issuing a dynamic response for
the next pick-and-place action. Instead of becoming familiar with a 2D drawing, the robot calibrates to a CAD
model and triangulates the position of the item in real-time. Intelligent robotics learns and optimizes the best
way to grab the item over many repetitions of picking up the product. The accuracy of the image location in
space coupled with a view of the product’s structural integrity enables the robotics to improve
continuously (and speed up) order fulfillment.
Outgoing Dimensional Inspection
3D-machine vision is ideal for measurement and dimensional inspection. It uses image sensors to record data in
the height, width, and depth dimensions and locates the position from the remaining
degrees of freedom on the yaw, pitch, and roll axes. This approach yields the enhanced accuracy required
for tightly tolerance control plan dimensions. 2D inspection compares a flat image of a part to a 2D engineering
drawing or known set of measurements. With 3D imaging, a picture of the shape, volume, or depth position of an
object or feature augments the benefits of 2D.
A common challenge in 2D inspection is a feature that does not meet the specification in either the depth or
rotational position normal to the viewing surface. A planar view might not catch an excessive deviation from the
dimensional tolerance, passing a part that should be rejected and flagged for the operator to check with the
process or equipment. 3D-machine vision collects positional data along all six degrees of freedom and builds the
image to address this challenge. The inspector’s confidence is higher with the added amount of data
analyzed as the robotics compares multiple versions of the picture. The software then superimposes them to
output a singular perspective of the relevant part or feature in real-time with intelligent robotics in a
process that does not require human intervention.
Defect Identification
If pick-and-place requires a macroscale level of accuracy and dimensional inspection calls for a microscale
level, part-defect identification needs one on the nanoscale. Throughput rate and fit/form/function are
essential, but a defective product compromises your company’s reputation and image. Consumers and
customers are only too happy to leave a negative review if a product is faulty. The marketplace is too advanced
to compromise on product integrity, and a product defect that the quality engineers cannot detect presents an
enormous risk of losing share.
The multitude of approaches to collect 3D images of a part can also describe the geometry and location of a
product defect. These defects can be expressed as unexpected density inconsistencies because of material
non-homogeneity, broken interior features, or residual support material remaining in an additively manufactured
part, or anything in between. In addition to dimensional accuracy, quality-assurance engineers can define a set
of success criteria to approve the part. A defective part could increase the scrap rate, reduce throughput, and
risk field failures if the engineers do not address it. 3D-machine imaging collects, analyzes, and transmits
information to the operators who immediately alert them of the issue. The data collected by the robotics
provides the engineers valuable, real-time data that they can use to summarize the frequency, consistency, and
placement of the defects for root-cause analysis. Early identification of a product defect is critical to
de-risking production and maintaining the manufacturing timeline.
Takeaway
As with any high-volume, capital-intensive process, the machines wear over time. This reality means that you need
to plan for unexpected process variables disrupting production. Machinery that uses this disruptive technology
can absorb unforeseen variables and obstacles, navigating them and completing their task without reprogramming.
The more information you can get during operation, the more likely you can get to a solution sooner.
3D-machine vision is a strong ally in this quest for more informed process conditions. It collects significantly
more data than its 2D counterpart and uses it to create and implement full images during mass manufacturing.
These images can help guide the machines to converge pick-and-place application positions and improve outgoing
dimensional inspection by adding insight into the depth and rotational axis directions. They can also identify
massively harmful product defects that could lead to recalls or safety issues.
3D machine vision is gaining popularity as part of the Internet of Things (IoT) by executing dynamic response
without reprogramming. Not yet wholly mainstream, the technology will rapidly go from novel innovation to
commodity expectation. Businesses will continue to push the feedback loop between machine and process control to
become shorter. The power of this technology will continue to grow because more industries and
mass-manufacturing processes connect.
Author Bio
Adam Kimmel has nearly 20 years as a practicing
engineer, R&D manager, and engineering content writer. He creates white papers, website copy, case studies, and
blog posts in vertical markets including automotive, industrial/manufacturing, technology, and electronics. Adam
has degrees in Chemical and Mechanical Engineering and is the founder and Principal at ASK Consulting Solutions,
LLC, an engineering and technology content writing firm.