Go 0 to 360 with Infineon Technologies' TLE5012B Magnetic Angle Sensors Now at Mouser
June 1, 2015 - Mouser Electronics, Inc., the global authorized distributor with the newest semiconductors and electronic components, is now stocking the TLE5012B GMR-Based Angle Sensors from Infineon Technologies. Based on an integrated Giant Magneto Resistive (iGMR) technology, the TLE5012B series combines magneto resistive sensing elements with integrated circuits all in one chip. These magnetic angle sensors offer high angular accuracy and resolution and can determine the absolute orientation of a magnetic field over the full range between 0° and 360°.
The Infineon TLE5012B GMR-Based Angle Sensors, available from Mouser Electronics, are designed for energy-saving motor control applications. TheTLE5012B sensors operate on a supply voltage of 5V, and help in directly measuring rotor angle, which can increase efficiency, reduce vibrations, and cut noise levels to ensure smoother motor integration. The sensors are equipped with a bi-directional, 3‑pin Synchronous Serial Communication (SSC) interface that is SPI compatible. Additionally the TLE5012B offers four other interfaces: Pulse-Width-Modulation (PWM) Protocol, Short-PWM-Code (SPC) Protocol, Hall Switch Mode (HSM) and Incremental Interface (IIF), all of which can be used in parallel with SSC or on their own.
The TLE5012B series of magnetic angle sensors feature extended data-processing functions, several user-selectable interfaces, and a 42 μs update rate — all helping to minimize delay time and provide high signal resolution. The integrated signal processing reduces the load of the microcontroller by performing precise angle calculations and calibration algorithms. The TLE5012B devices offer an angle accuracy of 1° with 15-bit resolution over the entire functionality range. All magnetic angle sensors within the TLE500x/TLE501x family offer extremely rapid updating and high efficiency and are automotive qualified. The devices are available through Mouser Electronics in a dual small outline (DSO) 8-pin package, and are ideally suited for a broad array of sensor and motor control-based applications — especially brushless DC (BLDC) motor drives.
To learn more about each of the three series of Infineon magnetic angle sensors, visit http://www.mouser.com/new/Infineon-Technologies/infineon-tle500x-tle501x-sensor/.
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 20 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About Infineon Technologies
Infineon Technologies is a leading global designer, manufacturer and supplier of a broad range of semiconductors used in various microelectronic applications. Infineon's product portfolio consists of logic products, including digital, mixed-signal, and analog integrated circuits, as well as discrete semiconductor products.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com